Sparks Electrical Supply | Industrial Lighting Distributor | Graybar
  1. Home
  2. Locations
  3. Graybar Sparks

Graybar Sparks

Address
150 E Greg St Ste 107
Sparks, NV 89431-7140
Contact

775-332-5200

775-332-5222

Hours
Sunday: Closed
Monday: 7:00AM–4:00PM
Tuesday: 7:00AM–4:00PM
Wednesday: 7:00AM–4:00PM
Thursday: 7:00AM–4:00PM
Friday: 7:00AM–4:00PM
Saturday: Closed
Sunday: Closed
Monday: 7:00AM–5:00PM
Tuesday: 7:00AM–5:00PM
Wednesday: 7:00AM–5:00PM
Thursday: 7:00AM–5:00PM
Friday: 7:00AM–5:00PM
Saturday: Closed
Sunday: Closed
Monday: 7:00AM–5:00PM
Tuesday: 7:00AM–5:00PM
Wednesday: 7:00AM–5:00PM
Thursday: 7:00AM–5:00PM
Friday: 7:00AM–5:00PM
Saturday: Closed
Sunday: Closed
Monday: 7:00AM–5:00PM
Tuesday: 7:00AM–5:00PM
Wednesday: 7:00AM–5:00PM
Thursday: 7:00AM–5:00PM
Friday: 7:00AM–5:00PM
Saturday: Closed
After Hours

1-800-GRAYBAR (472-9227)

4:00AM—8:00PM

6:00AM—3:00PM

Social Media
Graybar Sparks

Graybar Sparks, NV, is one of more than 260 North American locations for Graybar, the leading commercial and industrial lighting supplier in the country. The distribution of high-quality electrical supplies and energy products is our specialty. 

Keeping costs down is the goal of every commercial operation in existence. When lighting accounts for more than 20 percent of energy used in commercial buildings today, significant savings can be had by reducing energy costs. Most businesses see a return on investment in two years or less. Whether retrofitting an existing building, or starting a new construction project, Graybar Sparks offers comprehensive lighting and energy solutions. 

By swapping out old lamps and ballasts, installing new LED technology in the existing fixture housing, and adding or upgrading lighting controls, energy use can be cut by up to 67 percent. Over time, these energy savings can be significant enough to not only pay for the new equipment, but actually produce a return on investment. Typical ROI for our customers is between 17 and 45 percent. 

When designing new projects, implement complete building systems that will reduce energy costs from the very start. When designed and implemented correctly, daylighting uses natural light from windows and skylights to offset electrical loads. Coupled with intelligent control boards, occupancy sensors, manual and automatic dimmer switches, and time scheduling, these design features create a modern solution to keep energy costs low. 

Because of the hazardous waste contained in old lighting and electrical supplies, Graybar takes recycling very seriously. Today’s modern technology is far more efficient and environmentally-friendly than before, but the proper disposal of lighting waste will keep your business free of the liability and negative publicity involved with potential federal violations. 

Trusted since 1869, Graybar should be your top choice for a commercial and industrial lighting supplier.