Milwaukee News

  • Milwaukee M12 HAMMERVAC

    Compatible with major power tool brands of SDS plus rotary hammers and AC/DC hammer drills, the M12 HAMMERVAC universal dust extractor is the industry’s only universal dust extractor.

    07/29/2013

  • Milwaukee M12 FUEL Hammer Drill

    Milwaukee's M12 FUEL Hammer Drill is engineered for the most demanding tradesmen in the world. The M12 FUEL delivers unrivaled performance in a compact structure and features three Milwaukee-exclusive innovations that deliver unmatched power, run time and durability.

    04/18/2013

  • Milwaukee M12 1/2" SDS Hammer

    Four out of every five holes drilled in masonry are with 1/2" or smaller bits, making the new compact M12™ 1/2" SDS Hammer from Milwaukee Tool capable of handling 80 percent of all masonry drilling tasks.

    10/02/2012

  • Milwaukee M12 Cable Cutter Kit

    Using a break-through powered ratcheting mechanism and superior blade geometry, The Milwaukee M12™ Cable Cutter cuts through large cables with ease, leaving a clean, installation-ready cut.

    10/02/2012

  • M18™ Cordless LITHIUM-ION Band Saw Kit

    At only 10-1/4 lbs. and 18" in length, the M18™ Cordless LITHIUM-ION Band Saw Kit is the perfect tool for cutting metal in-place, overhead or in tight spaces.

    07/18/2012

  • Milwaukee 2210-20 Fluorescent Lighting Tester

    The Milwaukee 2210-20 Fluorescent Lighting Tester is a new world tool that tests fluorescent lighting fixtures and cuts troubleshooting time in half. The Fluorescent Lighting Tester delivers complete Lamp, Ballast and Pin testing. Test Lamps before or after installing, and test without dismantling the fixtures.

    01/20/2012

  • Milwaukee M18™ Combo Hammer Drill/Impact Kit

    The 2697-22 M18™ 2-Tool Cordless LITHIUM-ION Combo Kit includes the ½" Hammer Drill Driver (2602-20) and the ¼" Hex Compact Impact Driver (2650-20). The M18™ Cordless System's patented technologies and electronics, innovative motor design, and superior ergonomics provide the most efficient blend of power, weight and performance in the industry.

    09/26/2011

  • Hard-Hitting Hammers Last Longer, Work Faster

    If you thought a one-size-fits-all hammer could handle all the jobs you do, consider SDS Plus Rotary Hammers from Milwaukee Tool and Graybar.

    07/11/2011

  • Fast and Compact, the M18 Cordless 5-3/8" Metal Saw Delivers Power and Portability

    Cut metal faster and more accurately than ever before with the latest addition to the M18™ Cordless System: the M18™ 2682 Cordless 5-3/8” Metal Saw from Milwaukee and Graybar.

    04/13/2011

  • Compact Hammer Drill Provides Maximum Performance To Get The Job Done

    The M12™ Cordless 3/8" Hammer Drill Driver is the industry's first sub-compact hammer drill driver. At only 7-5/8" long and 2.8 lbs, it is the lightest and most compact hammer drill driver on the market, making it ideal for contractors, maintenance technicians, and re-modelers desiring maximum portability with the performance to get the job done.

    01/06/2011