L.H. Dottie proGrabit Screw Removal Tool and ShaftLok 15-in-1 Screwdriver Video

L. H. Dottie proGrabit screw removal tool helps contractors remove any damaged screws embedded in the wall or in metal products. It has two ends: one is the cutting end and in reverse it will make a conical-shaped hole in the screw that’s stripped. The other end of the proGrabit screw removal tool will mate its own threads going in – in reverse- and once it bites in and meets those threads it connects to the screw and will remove it out of the embedded base material.

L. H. Dottie also demonstrates the Shaftlok 15-in-1 screwdriver. This screwdriver incorporates a locking device where the shaft connects to the tips and without releasing it, the bit will stay in place. The Shaftlok 15-in-1 screwdriver also includes extensions to help reach areas high above, far below of inside a panel. It allows you to lock the shaft in place. The Shaftlok 15-in-1 screwdriver tool incorporates seven double-ended tips – flat, Phillips, tork and square drive. It is one tool that acts as 14 different screwdrivers.