DataComm Updates

DataComm Updates
  • Fit 48 Ports of Connectivity in one Rack with Legrand's High Density Connectivity Line

    Legrand's high density connectivity line has a range of mounting options, both at the panel and the work station.


  • Everything IP: Protecting Your Network Traffic

    Berk-Tek has identified three interrelated market drivers that are pushing the advancement of new technology. The question is: Will your network infrastructure hold up?


  • Preparing for the New Normal: IoT (Internet of Things)

    Important decisions must be made about whether to build or maintain an enterprise data center, lease colocation space or take the data center to the cloud as storage demands, security needs, data-processing speeds and data volume all increase. Read more.


  • Belden's new RJ45 REVConnect Connectivity System

    REVConnect is a brand new RJ45 connectivity system from Belden. A single Reliable and Easy termination method that offers unparalleled Versatility; it covers jack and plug, shielded or unshielded, Category 5e through Category 6A. Read more.


  • Efficient Data Center Cooling and Climate Management in the Age of the IoT

    With the continuous advancement of cloud computing and the evolution of the Internet of Things (IoT), modern enterprise data centers are having to push limits to provide uninterrupted service of the highest quality. Data center managers have to be more proactive than ever, restructuring their strategies to allow for greater capacity and expansion across the various areas of IT infrastructure. Read more.


  • The Scalable, Easy-Install Solution For Mission-Critical Networks: Atlas-X1 Connector From Leviton

    With easy network installation, industry-leading performance, and total scalability, the Leviton Atlas-X1 UTP Connector was built with you and your customers in mind. Tool-free termination means installers won’t spend hours on tedious, repetitive tasks. The Atlas-X1 is easily scalable for migrations up to 40GBASE-T, and delivers the highest level of verified performance and reliability. That means fast deployment and exceptional versatility. Read more.


  • Five Reasons Upgrading to Versiv Will Save You Money

    Learn five simple reasons why you should upgrade to Fluke Networks’ Versiv cabling certification system which is designed to save you even more money and to get to systems acceptance faster. Read more.


  • Evolution of In-Building Networks

    Local area networks and in-building wireless needs are evolving. Smarter buildings and demand for data require robust networks. Fiber-based networks provide a unique value proposition by bringing network access and intelligence closer to end-users. Watch this webinar on demand.


  • Power is the New Signal

    Cabling performance has been measured historically in terms of information capacity. A new LAN deployment strategy called Direct Connect can maximize PDE by effectively connecting equipment to end devices with a channel made entirely with horizontal cabling. Direct Connect does require the attachment of a plug and testing in the field. New developments in the standards is available to make this a practical deployment strategy and offer an efficient method to deliver data and power to end devices.


  • [VID] Video: A Great Solution to Extend Video from Hubbell with 110 Everywhere

    Hubbell's 110 Everywhere solution has gone to a 4 pair standard, and on the back of the modules to extend A/V is the 110 connector.