Home | Locations | Careers | About Us | Contact Us | Logon | Help
Product Search   [Advanced Search]
Asterisk (*) may be used as wildcard
Realize Relight with Graybar

Relighting Brings Color to Black-and-White Solutions

If you would like to see a visual difference in your space, coupled with remarkable energy savings, realize that you don't have to live with black & white answers.

RELIGHT fixtures from Graybar, Lithonia Lighting and GE can bring your existing space into vibrant color and help you realize your facility's potential.

Relighting Brings Color To Black and White Solutions

Resources

Realize Relight

Free copy of the Relight Solution guide

REALIZE RELIGHT

The RELIGHT Solution

With our relight solution, occupants will notice a marked improvement in how their space looks and feels. Your company will enjoy savings and reduced maintenance costs in a greener, more sustainable building. These goals can be accomplished cost effectively and with minimal disruption to your business.

The RENOVATION challenge

Renovating your lighting should deliver:

Revitalized look of the space

Enhanced lighting quality

Reduced energy and maintenance costs

Greener, more sustainable operation with minimal disruption to your business activities

 

TRADITIONAL solutions fall short:

RELAMPING with lower-wattage components will reduce energy consumption, but leaves the dated look of existing fixtures which often are dirty and fingerprint-laden.

RETROFITTING with specular reflectors and a reduced number of lamps lowers maintenance requirements and saves energy, but creates harsher, more focused light that degrades the lighting environment in addition to leaving the dated louver in place. And, your solution may not be UL listed.

REPLACING existing fixtures delivers energy savings, refreshes the space and delivers enhanced quality of light. Unfortunately the removal of existing fixtures and demolition required disrupt normal business activities. In addition, replacements generate the extra expense of more labor and entirely new fixtures.

HOW is it done?

REUSE

Reuse the fixture housing and wiring in place with the new assembly

Reuse the fixture housing and wiring in place with the new assembly. Keep the space clean by not removing the ceiling tiles.

« Previous | Next »

REDUCE

Upgrade internal fixture components with relight assembly containing fewer, longer-life lamps - and reduce your energy use by as much as 67%

Upgrade internal fixture components with relight assembly containing fewer, longer-life lamps - and reduce your energy use by as much as 67%

« Previous | Next »

RECYCLE

Recycle aluminum louver, channel cover, lamps and ballasts in an environmentally friendly way

Recycle aluminum louver, channel cover, lamps and ballasts in an environmentally friendly way.

« Previous | Next »

REVITALIZE!

REVITALIZE

« Previous | Next »

 

WHAT are the options?

The New RT5R
The New ES8R
The New I-BEAM

The New RT5R®

Ideal one-for-one replacement

35 - 55% energy savings

0.72 watts per square foot

Improves appearance

2x4 or 2x2 configurations

Featuring GE UltraStart T5 Lamps & Ballasts

Parallel Lamp operation extends relamping 15%

RoHS compliant - Reduction of Hazardous Substances

The New ES8R™

Ideal one-for one replacement

45 - 67% energy savings

0.60 watts per square foot

Shielded comfortable lighting

Featuring NEMA Premium® / GE UltraMax® Ballasts & T8 Lamps

2x4 or 2x2 configurations

Parallel lamp operation extends relamping 15%

RoHS compliant - Reduction of Hazardous Substances

The New IBU

Ideal one-for-one replacement of HID

Requires no disassembly to hang

Easier to handle due to narrow width

Uses about half the energy of a conventional 400-watt high bay

Fast starting 700 milliseconds

90°C Case/55°C(131°F) Ambient UltraCool

Parallel operation can extend relamping up to 15%

RoHS compliant - Reduction of Hazardous Substances