News

  • [VID] Save up to 90% Labor Time by Using Integrated Equipment from Schneider Electric

    Integrated Equipment from Square D by Schneider Electric is truly one of the best time-savers for labor that you can find in the industry. It takes your panels and transformers and combines them into one unit, so that you're not having to go out in the field and wire that and bend all those conduits.

    11/30/2016

  • [VID] Schneider Offers Short Circuit Coordination and Arc Flash Studies

    Schneider Engineering Services include short circuit coordination and arc flash studies. Each state has different licensing requirements and Schneider Electric has multiple licensed engineers in almost every single state.

    11/28/2016

  • Compact, Flexible & Easy To Install: EZ Meter-Pak Meter Centers From Square D By Schneider Electric

    After a long day, sometimes you feel like hogging all the elbow room on the train ride home. But when you’re installing meter centers in a high-rise building, a bulky, space-hogging install is more problematic than a few sideways glances. Luckily, Square D has a line of EZ Meter-Pak™ Meter Centers that are not only more compact than traditional units, but also more flexible and easier to install.

    09/05/2016

  • The Whole House Surge Protection Solution: Square D Home Electronic Protective Device (HEPD80)

    For the whole-home surge protection your residential customers demand, trust HEPD80 from Square D. With the average home containing $15,000 of unprotected personal electronics, home appliances, and electrical equipment, a high surge of power can cause serious damage. On their own, surge-protective panels and power strips aren’t enough to prevent power surges, leaving appliances and electronics vulnerable. Let Square D take it from here.

    04/20/2016

  • Reliable, Safe & Easy: QO & Homeline Plug-on Neutral Load Centers From Square D by Schneider Electric

    Arc and ground fault hazards lurk in the dark corners of every home. Like superhero and sidekick, the Homeline Plug-on Neutral CAFI Circuit Breaker and Load Center System keeps homes everywhere safe. Plus, electrical contractors will save time on installation, and meet NEC’s arc and ground fault requirements in a single bound. Square D is here to save the day.

    04/01/2016

  • Meet Title 24 Requirements With Ease: Homeline Solar-Ready Plug-On Neutral CSEDs

    To meet Title 24 requirements, trust Homeline’s Solar-Ready Plug-On Neutral CSEDs. Adhering to electrical code and getting off the job quickly is all in a day’s work. But contractors working in California, Phoenix, Las Vegas, or Seattle must now meet Title 24 requirements to equip homes for new and future solar installation. One step ahead, Schneider designed the first and only solar-ready, plug-on neutral CSED.

    08/25/2015

  • Save Space and Time with TeSys N Self-Protected Combination Motor Controller From Square D

    On the plant floor, every motor, cog, and turning gear serves a purpose—and there’s no room for error. To keep operations chugging along, electrical contractors and installers need a motor controller that’s durable and easy to install, access, and maintain. With robust performance and an efficient design, the TeSys™ N Self-Protected Combination Motor Controller delivers on all fronts.

    05/12/2015

  • Minimized Floor Space + Labor Savings = Schneider Electric’s Square D IPC2™ Transformer Combo (IPC2X)

    How would you like electrical equipment to arrive? Piece by piece, or in one neat package? Rising installation and labor costs are real. To deliver on time and on budget, integrated equipment does the job without eating up valuable resources. With Schneider Electric’s Square D IPC2™ Transformer Combo (IPC2X), you’ll minimize floor space, reduce installation costs and labor, and shorten cycle times.

    11/13/2014

  • Time-saving Square D QO and Homeline Dual-Function Circuit Breakers

    Meeting code requirements is a big part of your job. Square D QO™ and Homeline Dual Function Circuit Breakers from Schneider Electric reduce costs by combining two critical, state-of-the-art technologies—Combination Arc Fault and Class A Ground Fault protection—into one code-compliant, easy-to-install circuit breaker.

    09/24/2014

  • [VID] Schneider Electric Magelis SCU

    Schneider Electric provides you Magelis SCU, the latest generation of HMI controllers. Now you can drive and monitor all of your machines in a single product while reducing your machine assembly and energy costs.

    07/31/2014