It Takes a Remote Display Multimeter and Clamp Meter to Get the Job Done - Conveniently and Safely

Simultaneous voltage and current measurements are part of troubleshooting. And to be an effective troubleshooter, busy industrial and commercial electricians and electronic technicians need two meters: one to measure electrical current and one to measure voltage – specifically, the Fluke 233 Remote Display Multimeter and Fluke 381 Remote Display True-rms AC/DC Clamp Meter with iFlex™. Together, these two must-have tools boost productivity by allowing one person to complete a test that would have required two people using ordinary test tools.

Detachable displays make it possible to physicallyseparate the meter-positioning and resultsreadingfunctions, so you can pay attention to each task and reduce hazards. In addition, if the test location is hard to reach or in a dirty or noisy environment, the Fluke 233 and Fluke 381 let you set up the meter and then move toanother location to view and record test data.

Fluke 233 Multimeter: State-of-the-Art and Safe

Now, instead of being dangerously close to lethal electrical and mechanical forces, you can place the Fluke 233 with detachable wireless display where it's needed for testing – but view the test readings from a safe, convenient spot.

04/11/2011

Fluke 381 Clamp Meter: Convenient and Flexible

Simultaneous voltage and current measurements are part of troubleshooting. And to be an effective troubleshooter, busy industrial and commercial electricians and electronic technicians need a meter to measure voltage – specifically, the Fluke 381 Remote Display True-rms AC/DC Clamp Meter with iFlex™.

09/22/2011