Graybar and ERICO

Innovation and Quality

The Cornerstones of Our Business

Erico Corp HQ building image

For more than 100 years, ERICO has built its reputation by developing and marketing high-quality, innovative products. As a trusted industry leader, our products and services are recognized for providing labor and cost-saving solutions for customers throughout the world. It is our goal to continue to create high-quality, state-of-the-art products, while also providing the unparalleled service our customers have come to expect.

ERICO is a leading designer, manufacturer and marketer of precision-engineered specialty metal products serving global niche product markets in a diverse range of electrical, construction, utility and rail applications. The company is headquartered in Solon, Ohio, with a network of sales locations serving more than 25 countries and with manufacturing and distribution facilities worldwide.

ERICO’s products are marketed and sold under three premier brand names, which are recognized worldwide: CADDY fixing, fastening and support products; ERICO electrical grounding, bonding and connectivity products; and LENTON engineered systems for concrete reinforcement.

Erico brands image

Latest News and Articles

ERICO News

  • Reduce Your Total Cost of Install (TCI) in a Snap: CADDY’s Snap-to-Stud Electrical Box Bracket

    Would you clean your driveway with a toothbrush or blast it with a pressure washer? Unless you’re trying to conserve water, we bet you’d choose the latter. Spending excessive amounts of time and energy to install traditional electrical boxes isn’t exactly practical either. Introducing CADDY’s Snap-to-Stud Electrical Box Bracket, with a self-leveling feature to ensure the electrical box is always square to the stud before permanently mounting. With CADDY’s Snap-to-Stud Electrical Box Bracket, you’ll get the job done in a snap.

    12/07/2016

  • Save Your Equipment, Save Your Money: ERICO SES40P Surge Protective Devices

    ERICO’s new and improved SES40P Surge Protective Devices are an affordable option for protecting your equipment from dangerous transients and surge events. With its compact, convenient design, the SES40P device is easy to install and can be implemented in small spaces or by mounting the device to a panel. Whether your installation is commercial, industrial, or residential, this surge protective device offers consistent protection against damaging surges.

    08/04/2016

  • Electrical Boxes That Are Ready Right Away: CADDY Electrical Assemblies

    Electrical contractors know that every minute saved in installation and maintenance is a boon for convenience and savings. Ready to use straight out of the box, the CADDY ALL-IN-ONE Electrical Assemblies require just two screws for installation - no special tools or training necessary. Offering solutions for between-stud, stud-mounting, and floor-mounting installations, CADDY ALL-IN-ONE Electrical Assemblies are an efficient option for any electrical installation.

    07/07/2016

  • The Complete, Un-Corrodible Connection: ERICO CADWELD PLUS

    The tools required for your welding needs have been reduced to one: ERICO CADWELD PLUS. Featuring an entirely self-contained unit that requires no external ignition source, ERICO CADWELD PLUS creates connections that do not corrode, loosen, or increase in resistance. Designed for simplicity and ease-of-use, this solution for electrical connections reduces installation times by up to 20% and significantly reduces the risk of misapplication. Simplify your welding with a surefire solution!

    06/25/2016

  • CADDY C-Series and STS2346 Electrical Box Mounting Brackets

    The CADDY​ team is excited to announce the launch of two great new additions to their line of In-Wall Fastening products. The C-Series and STS2346 products were developed utilizing direct feedback from commercial electricians and continue CADDY's mission to provide superior value to you. ​ Read more.

    03/15/2016

  • The Easy-Install, Low-Hardware, Pathway-Support Solution: CADDY CAT HP J-Hook System

    Datacom customers need the capacity and solutions to support requirements for high-performance data cables. Electrical and datacom contractors must deliver on these needs while minimizing total hardware and labor costs. The CADDY CAT HP J-Hook System provides the performance, time savings, and versatility that today’s datacom and electrical contractors rely on.

    08/03/2015

  • CADDY ROD LOCK Threaded Rod Mounting System

    Consisting of a beam clamp, and anchor screw and a channel nut with an integrated washer, the CADDY® ROD LOCK Threaded Rod Mounting System eliminates many of the steps needed to create trapeze assemblies. Installers simply push threaded rods into CADDY ROD LOCK beam clamps and channel nuts – there’s no need to spin the rods into traditional clamps, or to spin multiple pairs of hex nuts and washers to secure struts.

    06/23/2015

  • The Hard-To-Steal Cable: ERICO CU-BOND Composite Cable

    From fiber optics to electrical and plumbing, copper has many uses. That’s why the resale value is highly lucrative on the black market. But thieves who think they’re taking the easy way out have another thing coming. ERICO’s CU-BOND Composite Cable—difficult to identify and cut—gives thieves a run for their money.

    05/18/2015

  • [VID] Speed Up Installation with ERICO CADDY SPEED LINK Universal Support System

    This video demonstrates how simple the ERICO CADDY SPEED LINK Universal Support System is to use and how easy it is to adjust the height up and down. The advantage of the CADDY SPEED LINK Universal Support System is that you can do installations of cable tray, wireless access points, speakers and a lot of electronics and devices. It speeds up installations 50 to 60 percent versus the threaded rod and jack chain applications.

    09/03/2014

  • [VID] Save Up 70% Installation Time with CADDY Rod Lock Threaded Rod Mounting

    ERICO's CADDY Rod Lock Threaded Rod Mounting System allows for the quick installation of threaded rod into beam clamps and strut nuts. Video demonstrates how you can take a threaded rod and simply push it into the beam clamp as opposed to threading it in. Additionally telescoping strut brackets can be pushed up on the threaded rod without having to screw them on, so it saves 60 to 70 percent of the labor time to do an installation.

    08/28/2014

Archived News