Archived Articles

  • [VID] Save up to 70% Set Up Time with a Reel within a Reel

    Encore Wire has a reel payoff and the reel payoff is our reel within a reel. We offer this starting on a 24" and go up to a 48" reel. As you can see, the inner drum interlocks from some steel pins and allows it to free spin as the contractor is pulling. So if you have a parallel with pulling heads, this actually comes on a 4-way pallet so it can be dropped directly on at the jobsite and is ready to pull.

    12/29/2014

  • Encore Wire Photovoltaic Wire

    Photovoltaic (PV) wire has superior sunlight resistance and low-temperature flexibility in addition to a thicker insulation or jacket and a proven level of flame resistance.

    04/12/2011