L. H. Dottie and Graybar

Since 1965 the L.H. Dottie Company has established a reputation for first class service and industry leading products. Today, the partnership between Graybar and Dottie continues that tradition. From fasteners & hardware, anchors & kits to tools & specialty items, the L.H. Dottie Company continues to provide a wide variety of quality products and an unrivaled level of customer service.

Latest News and Articles

Archived Articles

  • Strip Cables & Wires Quickly & Easily with Jokari Tools from L.H. Dottie

    Stripping cables can be a real drag. Switching from utility knives to wire strippers doesn’t just tire you out—it eats up valuable install time too. Lower your Total Cost of Install (TCI) and keep your mitts safe with L. H. Dottie’s line of Jokari tools. Jokari cable and wire strippers put versatility, safety, and precision into your hands.

    12/20/2016

  • The Hardworking, Heavy Duty Punch Kits: L. H. Dottie 12-Ton Hydraulic Punch Kits

    Boxing is often called the “sweet science,” since punches must be delivered with pinpoint accuracy and effortless execution. Working with steel isn’t much different—to come out on top, your punches must be efficient and accurate too. Step into the ring with Dottie’s 12-Ton Hydraulic Punch Kits. Punching holes through steel has never looked so easy.

    09/03/2016

  • The Never-Roll-The-Dice Ground Pigtail From L.H. Dottie Company

    You’re not one to shy away from a friendly game of Black Jack. When it comes to grounding? You never roll the dice. You’d wouldn’t dare improperly place ground receptacles, or skip GFCIs where required. But getting the job done properly isn’t a matter of knowledge alone—you need the right tools to get there. That’s where Dottie’s Ground Pigtails come in.

    12/03/2015

  • Your Go-To Solution For Light-Duty Drywall Mounting: Wall Driller Anchor Kits

    For lightweight anchoring in a variety of materials, trust Dottie’s Wall Driller Anchor Kits. On the surface, choosing a wallboard anchor doesn’t seem like an earth-shattering decision. But shortcuts aren’t your thing, and details matter. Choose the wrong anchor and you could find yourself with support and conductivity issues, and results you’re not proud of. Take a load off. Dottie’s got this.

    08/19/2015

  • L. H. Dottie Concrete Anchoring System

    Dottie's Concrete Anchoring System is faster to install than most conventional steel anchors. Hi-Low threads provide extreme holding strength and have the advantage of close to edge fastening without potential breakout.

    04/20/2015

  • [VID] Introducing L.H. Dottie’s first and only UL-listed pipe support system on the market

    Introducing L.H. Dottie’s first and only UL-listed pipe support system on the market. Pipe support system is made up of a light construction ABS and AES. It can be cut to length which saves the contractor money on the job. Budget requirements are what they are so this helps the contractor stay within budget. It’s a non-corrosive and high-UV rated pipe support system.

    12/15/2014

  • Reduce Costs, Not Performance, With Dottie’s Cut to Length Pipe Supports

    Material costs really add up. So why use more than you need? To keep your project budget in check, wrangling rising costs is crucial. You need a pipe support that does the job without the extra cost. With Dottie’s Cut to Length Pipe Support, you can use shorter lengths to achieve your design requirements. You do—and save—more with less.

    09/26/2014

  • [VID] L.H. Dottie proGrabit Screw Removal Tool and ShaftLok 15-in-1 Screwdriver

    L. H. Dottie proGrabit screw removal tool helps contractors remove any damaged screws embedded in the wall or in metal products. It has two ends: one is the cutting end and in reverse it will make a conical-shaped hole in the screw that’s stripped. The other end of the proGrabit screw removal tool will mate its own threads going in – in reverse- and once it bites in and meets those threads it connects to the screw and will remove it out of the embedded base material.

    08/22/2014

  • L. H. Dottie Zinc and Nylon, Quality Anchoring Kits

    L.H. Dottie’s first in class anchor kits provide users with a comprehensive mix of anchoring products. Several of Dottie’s most popular anchor kits include nylon anchors and Zinc Wall Board Anchors. 

    05/22/2014

  • L. H. Dottie First Aid Kits

    First aid kits from Dottie put reliable, professional-quality first aid at your fingertips. But the benefits extend beyond just the knowledge that help is always available.

    04/07/2014

Archived News