Graybar Livonia East

Graybar Locations

Through its distribution network of  North American locations, Graybar has become one of the leading commercial lighting suppliers in the United States. Founded in 1869, Graybar has since become one of the Fortune 500, and is one of North America’s largest employee-owned companies. By adding sophisticated logistics and project management operations to our services, we have become a vital link in America’s supply chain. Graybar Livonia East lives up to the reputation.

With more than 30 percent of energy used in commercial buildings wasted, a “smart” building is far more than a trend. It is an essential investment in the future. At the heart of these buildings is an infrastructure of lighting, communications, HVAC, and security systems operating from a single control system. Graybar can help you upgrade existing buildings, and plan new ones to be more energy efficient from the start.

Lighting retrofits are a simple, yet effective way to make an existing building more energy efficient. More than 25 percent of energy used in most facilities is used by lighting and increased efficiency will make a big impact on the monthly energy bill. Most electrical supplies will swap out directly with existing hardware and can use the old fixture housings to save time and ceiling repair costs.

When designing entirely new constructs, include energy-efficient features directly into your building from the get-go. Using an advanced network of occupancy sensors, dimmers, time scheduling, and intelligent control boards, your new building can start life as a “smart” structure.

If you need an end-to-end lighting solution, kitting for a larger project, or even a half-mile of raw conduit, Graybar Livonia East can deliver when and where you need it.

Google+  Tell us how we're doing by leaving a review on Google.
 

Graybar Livonia East

28188 Schoolcraft Rd.
Livonia, MI 48150

Location Type

  • Warehouse
  • Counter
  • Will Call

Contact

Phone: (734) 793-6820
Fax: (734) 421-8906
Emergency Number: 800-GRAYBAR (472-9227)

Location Hours

Mon-Fri: 7:00 am to 4:00 pm

Customer Service Hours

Mon-Fri: 5:00 am to 11:00 pm EST
Sat-Sun: 9:00 am to 6:00 pm EST