Graybar West Springfield

Graybar West Springfield, Massachusetts

Since 1869, Graybar has established itself as one North Americas leading commercial lighting suppliers, with  warehouse locations stocking thousands of high quality electrical supplies from hundreds of industry-leading manufacturers. When in need of end-to-end solutions for lighting projects, switchgear upgrade, a local or wide area network, or even a half-mile of electrical conduit, Graybar West Springfield has it, and we deliver it when and where it is needed.

Streamlining energy usage in commercial buildings is one of our key missions. Over 30 percent of energy used is done so inefficiently. Lighting upgrades can pay for themselves in as little as two years, and can even present a return on investment of up to 45 percent. Integrating Graybar PowerSmart® solutions can help you reach your long term sustainability goals like reducing 20% of your energy usage by 2020 as mandated by the federal government.

A lighting retrofit is a simple and effective way in which we can help make your buildings more efficient. Lighting retrofits not only increase the quality of light in a workplace, but also result in less heat, which in turn also reduces air conditioning costs. Retrofit fixtures install in minutes, swapping out lamps and ballasts to improve efficiency, and install directly into existing fixture housings. This cuts down on project turn around time and annoying ceiling tile repairs. There are plenty of reasons to consider a lighting retrofit in your building, and our lighting specialists can help answer even more questions about energy savings.

When new building projects are started, it would be wise to design them from the ground up to be energy efficient. Incorporating advanced control systems automatically take data from around the building using occupancy sensors and dimmers. With the added savings produced by integral day light sources designed into the structure, peak energy usage periods become lower in usage.

Graybar West Springfield offers a full array of electrical supplies, and the know-how to help you make use of them.

News and Events

  • Breakfast with Greenlee

    Join us and Greenlee representative Emily Sante for a counter day breakfast on Sept. 13, 2017. Enjoy coffee and donuts while hearing about the latest products and solutions. Plus, all in-stock Greenlee will be on sale!

    08/16/2017

Graybar West Springfield

31 Pearson Way
West Springfield, MA 01089

Location Type

  • Sales Office
  • Warehouse
  • Counter
  • Will Call

Contact

Phone: (413) 788-2030
Fax: (413) 732-2715
Emergency Number: 800-GRAYBAR (472-9227)

Location Hours

Mon-Fri: 6:30 am to 5:00 pm

Customer Service Hours

Mon-Fri: 5:00 am to 11:00 pm EST
Sat-Sun: 9:00 am to 6:00 pm EST