Graybar Bakersfield

Graybar Bakersfield, California

In a modern world with rising electricity costs, environmental concerns and the need for increased productivity, commercial operators everywhere are looking to streamline their energy consumption. Graybar Bakersfield is one of  locations that make up Graybar’s commercial lighting store network. Our Bakersfield branch is a full-service sales office, complete with warehouse, counter, and will call. The warehouse is stocked with thousands of high-quality electrical supplies from top-shelf manufacturers like General Electric, Philips and Acuity Brands. Graybar employs thousands of dedicated men and women and is one of the largest employee owned companies in North America.

Building “smart” buildings is what we do, and it’s more than a trend. Intelligent facilities are a sound investment in the future. At the heart of our buildings is an infrastructure of lighting, communications, HVAC and security systems operating over a single IP-enabled network. Our team of highly skilled technical specialists can help you plan and integrate a building-wide system that saves energy and is easy manage, both in your existing buildings and new construction projects.

When planning and designing a new building, there are several things our team can do to make it energy efficient from the start of its life. Effective daylighting uses natural light from skylights and windows to offset electrical loads during daytime. Designed and implemented properly, it can have a drastic effect on your monthly energy bill. Making use of motion controlled occupancy sensors, manual and daylight controlled dimmer switches, and time scheduling, your building won’t be wasting energy by lighting an empty room.

Retrofitting your building with new state-of-the-art electrical supplies is a simple and effective way to reduce the energy footprint. Swapping out lamps and ballasts takes minutes and the new fixture installs directly into the old housing. With these upgrades it is possible to reduce energy usage by up to 67 percent and the average return on investment seen by our clients is between 17 and 45 percent.

Graybar Bakersfield is the top-notch commercial lighting supplier you’ve been searching for.

Google+  Tell us how we're doing by leaving a review on Google.
 

News and Events

  • It Pays to Have Great Lighting

    The PG&E utility rebate program has just been updated to include a per fixture incentive based on $/kilolumen for eligible indoor, recessed fixtures.

  • Proposition 39

    California’s Proposition 39 Clean Energy Jobs Act provides roughly $550 million annually for five years for eligible projects that improve energy efficiency and expand clean energy generation in schools. The time is now to capture your share of these funds for building upgrades that will provide immediate energy savings and better performance for your school.

Graybar Bakersfield

6100 Schirra Court
Bakersfield, CA 93313

Location Type

  • Sales Office
  • Warehouse
  • Counter
  • Will Call

Contact

Phone: (661) 835-4300
Fax: (661) 832-4652
Emergency Number: 800-GRAYBAR (472-9227)

Location Hours

Mon-Fri: 7:00 am to 5:00 pm

Customer Service Hours

Mon-Fri: 5:00 am to 11:00 pm EST
Sat-Sun: 9:00 am to 6:00 pm EST