Berk-Tek Webinar: Pushing LAN Boundaries for Maximum Value

Pushing LAN Boundaries for Maximum Value

Those three drops 95m from the closet. The IP Camera or WAP that could use PoE, except that it is located a bit past the distances defined by the standard. The blue-light security phone that could be integrated into the rest of the system, but the specifics of how to accomplish it are a bit unclear.

We’ve all been there. But what exactly are your choices for extending your LAN to reach those devices that fall just beyond the standards?

Register for the Berk-Tek Webinar: Reaching Beyond the Distance and Performance Boundaries of the LAN, presented by industry experts Mike Connaughton and Jim Frey. This webinar will provide an insider’s look at best practices for reaching beyond the distance and performance standards of the LAN without sacrifice or peace of mind. Details to be discussed include:

  • What is pushing devices beyond the standard 100m Ethernet distances
  • Options to address these needs
  • Infrastructure recommendations for extended distances
  • Stretching the network backbone
  • Implications of extended distances at higher speeds, including 40G
  • Cost implications of various solution options
  • Presentation of DCCC Link Loss research and modeling
  • Launch of Link Loss Calculator
  • Product benefits of LANmark-2000, OneReach and GIGAlite-10XB
 
DATE
Thursday,
June 12, 2014
TIME
1:00 p.m. EDT
60-min Webinar
G2Talk Webinar Series Replay
REGISTER NOW